Skip to main content
 

STAMFORD® l AvK® has today launched two new products at the Middle East Electricity Show.

We are pleased to announce the launch of the new STAMFORD® S7 and STAMFORD® S9 which become the newest members of the STAMFORD®S-range of alternators. Both new alternators will be displayed publicly for the first time at the Middle East Electricity exhibition in Dubai from 5-7 March 2019 (stand number S2.B30).

The S-Range program was launched in 2016 and has seen five products released in the last three years (S0, S1, S4, S5, S6) before the introduction of these new alternators. These two brand new models build upon the success seen so far with this new range by answering the demands from the market for increased power densities and continuing to demonstrate the market leading capabilities that can only result from over 100 years of product innovation.

Designed using CoreCooling™ Technologies, the Low Voltage STAMFORD® S7 delivers now greater power density with continuous ratings up to 2.5MVA thanks to enhanced thermal management within the machine. This optimization also helps reduce machine dimensions and weight.

The compact design benefits from flexible feet for ease of integration into existing generating set designs, and brings with it upgraded Automatic Voltage Regulator options plus an overall design package that also offers improved field serviceability.

Watch the STAMFORD® S7 product launch video

The brand new STAMFORD® S9 is a High Voltage product that introduces with it true Class H insulation technology. Designed, tested and validated over an extended period, at component, subsystem and at whole machine levels, this new system can run continuously at Class H ratings of up to 5,000kVA, 13.8kV, whilst still delivering high resistance to the mechanical and thermal stresses seen in rotating machine applications.

The S9 product, built upon over 30 years’ experience of STAMFORD® l AvK® High Voltage product knowledge, also offers both weight and dimensional reductions, ease of integration into existing generating set designs, and improved field serviceability

Watch the STAMFORD® S9 product launch video

The new STAMFORD® S7 and S9 products also benefit from the market leading S-Range 3 Years Warranty as standard.